Machine Op II Stainless Weld - 2nd Shift
Marinette, Wisconsin, United States of America

Sie haben die Job-URL erfolgreich in die Zwischenablage kopiert!

Jobdetails

Beschäftigungsart: 

Full-Time

Standort:

Marinette, Wisconsin, United States of America

Jobkategorie:

Mfg Machine Operation

Auftragsnummer:

WD30248449

Stellenbeschreibung

QUALIFICATIONS
Must be 18 years of age and have a HS Diploma or equivalent. Must have reading, writing and simple math skills.  Must be able to read blue prints. Must have previous experience working as a Machine Operator I within Stainless Steel. Must have welding experience and knowledge of TIG welding as would be shown by the passing of a hands-on competency test; the knowledge one might get from a vocational school course is helpful.

DUTIES

  • Operates highly complex machinery used in the production process. From prints, adjusts and tig welds stainless steel shells and components.
  • Performs semi-complex machine set-ups; loads welder with component parts to be welded.
  • Ensures machines are operating at required capacity and that production requirements are met.
  • Monitors the performance of equipment; identifies, troubleshoots, and resolves problems in order to maintain efficient operations.
  • Observes machine operation to verify accuracy of machine settings and to detect malfunctions or out of tolerance production. Monitors controls of welder (temp, cycle time, amps-volts, etc.)
  • Recognizes process upset; both special and common cause, and notifies the appropriate person.
  • Assists in preparing and maintain scorecards, Gemba Boards, etc., so that performance problems can be identified and resolved.
  • Assists maintenance team in basic troubleshooting and equipment malfunctioning diagnostics.
  • Maintains equipment and performs preventive maintenance notifying Group Leader/Maintenance personnel if welding machine malfunctions.
  • Visually inspects welds to assure that blueprints, code and quality standards are met.
  • Supporting the training and development of peers within the organization.
  • Performs assembly, packaging, housekeeping and other related duties as may be assigned by the Group Leader or supervisor.

Bleiben Sie über die neuesten Stellenangebote auf dem Laufenden

Erhalten Sie kuratierte Stellenangebote direkt in Ihren Posteingang.

Abonnieren