Machine Op II Stainless Weld - 2nd Shift
Marinette, Wisconsin, United States of America

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Detalles del empleo 

Tipo de empleo: 

Full-Time

Ubicación:

Marinette, Wisconsin, United States of America

Categoría del empleo:

Mfg Machine Operation

Número de empleo:

WD30248449

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Descripción del empleo

QUALIFICATIONS
Must be 18 years of age and have a HS Diploma or equivalent. Must have reading, writing and simple math skills.  Must be able to read blue prints. Must have previous experience working as a Machine Operator I within Stainless Steel. Must have welding experience and knowledge of TIG welding as would be shown by the passing of a hands-on competency test; the knowledge one might get from a vocational school course is helpful.

DUTIES

  • Operates highly complex machinery used in the production process. From prints, adjusts and tig welds stainless steel shells and components.
  • Performs semi-complex machine set-ups; loads welder with component parts to be welded.
  • Ensures machines are operating at required capacity and that production requirements are met.
  • Monitors the performance of equipment; identifies, troubleshoots, and resolves problems in order to maintain efficient operations.
  • Observes machine operation to verify accuracy of machine settings and to detect malfunctions or out of tolerance production. Monitors controls of welder (temp, cycle time, amps-volts, etc.)
  • Recognizes process upset; both special and common cause, and notifies the appropriate person.
  • Assists in preparing and maintain scorecards, Gemba Boards, etc., so that performance problems can be identified and resolved.
  • Assists maintenance team in basic troubleshooting and equipment malfunctioning diagnostics.
  • Maintains equipment and performs preventive maintenance notifying Group Leader/Maintenance personnel if welding machine malfunctions.
  • Visually inspects welds to assure that blueprints, code and quality standards are met.
  • Supporting the training and development of peers within the organization.
  • Performs assembly, packaging, housekeeping and other related duties as may be assigned by the Group Leader or supervisor.

Mantente actualizado con las últimas oportunidades

Subscríbete a nuestro boletín de empleo para recibir las últimas actualizaciones sobre oportunidades profesionales, noticias de la empresa y perspectivas de la industria.

Subscríbete