Vous avez réussi à copier l'URL de l'emploi dans le presse-papiers !
Type d'emploi:
Emplacement:
Catégorie d'emploi:
Numéro de travail:
Description de l'emploi
QUALIFICATIONS
Must be 18 years of age and have a HS Diploma or equivalent. Certificate or 1-3 years of experience in all weld processes. Proficient at reading prints. Knowledge of arithmetic. Must pass 1G and 2G weld test (GMAW13) and /or any other code/customer quality related requirements. Arm-Hand Steadiness; the ability to keep your hand and arm steady while moving your arm or while holding your arm and hand in one position. Multi-limb Coordination; the ability to coordinate two or more limbs while sitting, standing or lying down. It does not involve performing the activities while the whole body is in motion. Manual Dexterity; the ability to quickly move your hand, your hand together with your arm, or your two hands to grasp, manipulate or assemble objects. Performing physical activities that require considerable use of arms, legs, moving your whole body, such as climbing, lifting, balancing, walking, stooping and handling of materials. Problem Sensitivity; the ability to tell when something is wrong or is likely to go wrong. It does not involve solving the problem, only recognizing there is a problem. Selective attention; the ability to concentrate on a task over a period of time without being distracted. The following training is required for this job position. Applicable Safety Training related to specific job tasks 80% minimum pass rate. ISO 9001 Quality Policy and all job specific procedures, work instructions, and use of applicable forms. Must pass 1G and 2G weld test (GMAW13).
DUTIES