Vous avez réussi à copier l'URL de l'emploi dans le presse-papiers !
Type d'emploi:
Emplacement:
Catégorie d'emploi:
Numéro de travail:
Description de l'emploi
The role is for Qualified Energy Auditor for the South India Region, based out of Hyderabad. The candidate will be responsible for conducting ASHRAE Level 1/2/3 Audits as required to develop Energy Conservation Measure (ECM). Should be well versed with benchmarking the system and aware on the BEE /ASHRAE and other Rating systems. The candidate should have relevant experience in the Audit and possess the quality to gather the data, analyze, interpret and conclude, including preparation of Report and Presenting to the stakeholders. The candidate is also responsible for generating opportunity for the identified ECM’s and other HVAC system, Controls and other system optimization, Performance Analysis of Equipment etc. Hands on experience for the Use of Flow meters, Power Analyzers, Temperature & RH meter, Psychrometer, Lux meter, etc. Measurement and Verification ( MVP)
Identify / Meet customer for retrofit & expansion opportunities. Work with sales team to qualify and conduct audit and develop investment grade report and presenting to relevant stakeholders. Conducting post implementation of Audit to demonstrate the Return-on-Investment ( ROI)
Candidate with 5-10 years Energy audit experience, good market connects with customers, in South India. Should possess positive attitude and quick learner. Travel as required for client meeting/site visit.
Should be BE/Diploma graduate. Certified auditor by BEE/LEED AP/CMVP is preferred.