What you will do:
This position will be responsible for the installation of complex integrated security systems to include the wiring, equipment and programming of access control systems, CCTV, digital recorders, network recorders, and intercom systems for clients.
How you will do it:
Capable of installing cabling, field equipment & control equipment enclosures in customer locations according to the national electric code, company and customer guidelines.
Can use electronic test equipment to troubleshoot complicated problems during installation.
Reads and interprets blueprints, diagrams, submittals, specifications, software/systems programs, schematics and operational product manuals.
Readjust equipment, repair or replace inoperative equipment and test for operation
Performs system checks for proper operation.
Knowledge of computer programs including word processing, spreadsheets and databases; CCTV and access control systems; media storage.
Ability to plan, organize and prioritize work paying close attention to details.
Ability to communicate effectively, orally and in writing, while establishing and maintaining cooperative working relationships.
Ability to analyze information.
Can work unsupervised to complete installation jobs and is self-motivated to complete jobs.
Completes and submits all necessary paperwork related to job assignments.
Capable of using hand and power tools to properly mount and secure equipment
Feed cables through access holes, roof spaces, and cavity walls to reach fixture outlets; then position and terminate cables, wires and strapping
Drill holes for wiring in wall studs, joists, ceilings, and floors.
Conduct End- User training.
Ability to isolate trouble to a customer network, where applicable.
What we look for:
Required
A Class D license in Massachusetts, also known as a Systems Technician license, is required to install and maintain electrical systems in homes and businesses, such as security alarms and fire warning devices. To obtain a Class D license, applicants must meet the following requirements:
Complete 300 hours of Board-approved education
Complete a 15-hour Code-Update Class
Gain 4,000 hours of work experience over a minimum of two years under the supervision of a licensed Systems Technician or Journeyman Electrician
Pass all licensure examinations with a score of at least 70%
Applicants must also submit the following documentation:
A certificate of completion for each learning objective
A letter of accreditation from the institution that provided the instruction
A description of coursework that includes the National Electrical Code, International Electrical Code, and any relevant regulations or codes
High school diploma, GED, or equivalent.
Significant background (3+ year experience) in Digital & Analog Camera Systems.
Significant background (3+ year experience) in Access Control Systems.
Understanding of the function and design of Alarm Systems.
Experience with IP addressable security devices (2+ years).
Must be computer literate to include advanced TCP/IP networking skills.
Must be able to operate a company truck with an acceptable driving record.
Is proficient with all aspects and operation of ADT A.I. core card access, CCTV systems.
Preferred
Associate degree or 2-year technical school program graduate preferred.
An industry-recognized apprentice training program may be substituted for the formal education requirement.
Specialized training/ certification in the following categories:
Access Control (at least 3 certifications from the following)
Prowatch
C-Cure 800 or C-Cure 9000
Casi- Facility Commander or Picture Perfect or Secure Perfect
CCTV- Analog (at least 1 certification from the following)
Bosch
Pelco
American Dynamics
Cisco
CCTV- IP (at least 1 certification from the following)
Genetec
Indigo Vision
Visitor Management (experience in any of the following preferred)
Honeywell Lobby Works
Stopware
Access Sentry
Additional experience a plus: MCSE, CCNA, Surveillance Systems, Intrusion Detection Systems, Perimeter Intrusion Detection Systems and Security Gate Operators.