Você copiou com êxito o URL do trabalho para a área de transferência!

Detalhes do trabalho

Tipo de emprego: 

Full-Time

Localização:

Nisku, Alberta, Canada

Categoria de trabalho:

Mfg Skilled Trades

Número do trabalho:

WD30245355

Você copiou com êxito o URL do trabalho para a área de transferência!

Descrição do cargo

Job Description 

 

Title: 

Journeyman Plumber 

Department: 

 

Reports To: 

Production Supervisor 

 

Overview 

The Journeyman Plumber will be responsible for the installation, maintenance and repairs associated with plumbing and heating requirements for a large manufacturing environment. He or she will work using safe work practices with items such as, but not limited to: air conditioning, humidifiers, gas lines, water pipes and sewer utilities in and about the facilities, as well as maintaining and repairing compressed air lines, compressors, and vacuum pumps. 

 

Roles & Responsibilities 

  • Installs commercial and in-house produced plumbing assemblies into in-process HVAC equipment. 

  • Reviews blueprints and specifications; ensures drawings and specifications will function as designed in environment intended for use and maintains drawings to reflect accurately any changes and/or additions that are made.  

  • Tends to plumbing, air, and vacuum issues to keep production equipment running.  

  • Participates in all construction and remodeling projects involving plumbing, air conditioning, or gas fitting changes and/or additions.  

  • Tends to the maintenance and preventative maintenance programs including cleaning for all plumbing, heating, and air conditioning, and air and vacuum related equipment.  

  • Proposes changes or modifications to plans to enhance production and efficiency of systems plans and specifications for sanitation facilities.   

  • Assist in training, directing,  and supervision of junior employees and apprentices, inspecting and certifying their work.  

  • Performs plumbing inventory and orders parts as required. 

  • Reviews coding accuracy of assigned builds.  

  • Provides technical Assistance/Emergency Response services to existing facilities.  

  • Set up and tests finished HVAC equipment for proper performance/customer requirements. 

  • Keeps detailed and accurate maintenance reports and safety documentation.  

  • Maintains a working knowledge of changes in technology, compliance, and repair techniques.  

  • Performs all duties in accordance with Silent-Aire Limited Partnership safety program standards and Alberta Occupational Health and Safety Act, Regulations, and Code. 

  • Other duties as required. 

 

Knowledge, Skills, & Abilities 

  • Completion of college/CEGEP/vocational or technical training preferred.  

  • Appropriate credentials and certifications - Industrial Plumber Trade Certification, 5th Period Apprentice, and working towards an Industrial Plumber Red Seal Certificate.   

  • Ability to work independently in a busy environment. 

  • Experience with routine maintenance operations. 

  • Highly flexible, with solid interpersonal skills that allow one to work effectively in a diverse working environment. 

  • Able to effectively communicate both verbally and in writing. 

  • Able to work well under pressure. 

  • Strong attention to detail. 

  • Able to deal with people sensitively, tactfully, diplomatically, and professionally at all times. 

 

Working Conditions 

  • 24/7 availability may be required. 

  • Physical ability to lift up to 50lb. 

  • Travel to off-site locations may be required. 

  • Always adhere to safety policies (wear protective equipment). 

  • Overtime as required. 

  • Hazards associated with the trade. 

  • Work both indoors and outdoors, may be exposed to construction sites. 

 

Contacts 

  • Communication is primarily internal to the assigned work team and Production Supervisor. 

 

Mantenha-se informado sobre novas oportunidades de emprego

Assine alertas de empregos para receber vagas selecionadas em sua região e mantenha-se informado sobre as últimas oportunidades de carreira na Johnson Controls.

Inscrever-se