Fire Alarm Installation Apprentice
Rocky Hill, Connecticut, United States of America

Você copiou com êxito o URL do trabalho para a área de transferência!

Detalhes do trabalho

Tipo de emprego: 

Full-Time

Localização:

Rocky Hill, Connecticut, United States of America

Categoria de trabalho:

Mfg Skilled Trades

Número do trabalho:

WD30238628

Você copiou com êxito o URL do trabalho para a área de transferência!

Descrição do cargo

What you will do
Fire Alarm Installation Apprentice is responsible for working in a team to complete the installation, of fire protection systems including: low voltage wiring and device installation for fire alarm, access control, security and suppression systems. Apprentices are also responsible for properly securing all Johnson Controls tools and equipment at the end of each work period so as to prevent damage or loss. 

How you will do it
Applies judgment based on practice and precedence.
Must be willing and able to follow directions when given.
Must be able to think ahead and keep the momentum of the task moving forward without direction.
Must maintain proper documentation for all work performed.
May review project drawings to obtain all facts necessary to perform installation activities according to specifications.
Must be able to work alternative shifts or weekends to meet customer and/or job requirements.
Must adhere to all company safety policies and procedures.
Must be comfortable working from heights.

What we look for
Required

  • Passing grade from appropriate trade school
  • Follow verbal and written instructions.
  • Capable of performing physical labor to include carrying and moving equipment and tools weighing up to 70 lbs.
  • Able to work in unusual and sometimes difficult positions such as climbing ladders, scaffolding and high lift equipment up to 60 feet, working within ducts, crawl spaces, above ceilings, etc.
  • Ability to work flexible hours.
  • Ability to adhere to, implement, and follow safety guidelines and procedures at all times.
  • Excellent communication skills, using tact and diplomacy when dealing with customers and team members.
  • Positive attitude, and an ability to learn quickly.
  • Possess a valid driver’s license and driving record that meets company requirements.
  • Able to pass a pre-employment background and drug test.
  • Able to obtain and retain any licenses required by National, State and Local codes.


Preferred

  • OSHA/MSHA/NICET Certifications

Mantenha-se informado sobre novas oportunidades de emprego

Assine alertas de empregos para receber vagas selecionadas em sua região e mantenha-se informado sobre as últimas oportunidades de carreira na Johnson Controls.

Inscrever-se