¡Has copiado correctamente la URL del trabajo en el portapapeles!

Detalles del empleo 

Tipo de empleo: 

Full-Time

Ubicación:

Manila, Manila, Philippines

Categoría del empleo:

Field Operations

Número de empleo:

WD30238785

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Descripción del empleo

What you will do:

The Chiller Operator ensures smooth and efficient function or performance of the chiller systems in the assigned project site while on duty. He/she must ensure the standard parameters are always met. In addition, he/she must have the knowledge on basic chiller troubleshooting, repair and preventive maintenance.

How will you do it:

  • Ensures on time opening and closing of chillers as per schedule

  • Inspects, monitors, and documents plant equipment and its function on an hourly or daily basis.

  • Maintains work area, equipment and chiller plant room in a neat and orderly condition

  • Reports all chiller concerns to the client and Project Engineer

What we look for:

  • TESDA NCII Certificate in Domestic Refrigeration or its equivalent

  • Has at least 1-2 year related work experience in chiller operatorship

  • Willing to be on assigned on shifting schedule and is open for relocation when needed

Mantente actualizado con las últimas oportunidades

Subscríbete a nuestro boletín de empleo para recibir las últimas actualizaciones sobre oportunidades profesionales, noticias de la empresa y perspectivas de la industria.

Subscríbete