HVAC O&M Specialist III
Grand Forks, North Dakota, United States of America

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Detalles del empleo 

Tipo de empleo: 

Full-Time

Ubicación:

Grand Forks, North Dakota, United States of America

Categoría del empleo:

Fac & Corp RE Management

Número de empleo:

WD30220995

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Descripción del empleo

RESPONSIBILITY LEVEL:

Under specific direction, this position assists in the production of, and maintaining of a uniform flow of steam by operating high-pressure boilers and maintaining all equipment in the boiler room.

PRINCIPLE DUTIES:

  • Assist in the operation and maintenance of a high pressure gas/oil fired boiler plant along with all associated equipment on a 24/7 based schedule to including weekends and holidays.
  • Control and adjust boiler fuel air mixture, pump pressure, tank levels, and other boiler plant related systems and equipment via automated control systems to ensure good-safe operation while maximizing boiler efficiency.
  • Assist maintenance staff with cleaning, repair and maintenance of boilers and associated equipment.  Includes fireside and waterside cleaning along with other maintenance duties assigned. 
  • Make entries into a daily shift log, updating fuel usage and maintenance reports.  Use of personal computer for maintenance records and data entry.  All other duties assigned.
  • Subject to call back to maintain shift coverage and overall plant operation.
  • Selects and lays out required materials per work orders or verbal instructions.
  • Sets up and operates tools and machines incidental to operations.
  • May be required to assist with requisitioning new supplies and equipment.
  • Performs all work in accordance with established safety procedures.
  • Complies with all company policies and procedures and adhere to company standards.
  • Perform other duties as required.
  • Must be a team player committed to working in a quality environment.

REQUIREMENTS:

  • Completion of a two year technical degree or equivalent, or a minimum of two years’ experience in the Maintenance and Operation field.
  • Requires knowledge of trade fundamentals sufficient to perform specialized service and repair work.
  • Requires ability to work in a team oriented atmosphere while being able to follow verbal and written instruction.
  • Must be physically able to perform basic maintenance tasks to the highest caliber, which includes ability to:  climb ladders, work in confined spaces, lift heavy objects weighing up to 50 lbs., etc.
  • Must be able to work varying shifts, weekends and holidays as needed. subject to callbacks seven day a week, 24 hours a day
  • Required to use a variety of hand and power tools or forklift.
  • May be required to possess a valid driver’s license.

PREFERRED:

  • Equivalent to a Special Class Minnesota Boiler Operator’s License or higher
  • Ability to work from drawing, diagrams, and sketches

#TechHiring

Mantente actualizado con las últimas oportunidades

Subscríbete a nuestro boletín de empleo para recibir las últimas actualizaciones sobre oportunidades profesionales, noticias de la empresa y perspectivas de la industria.

Subscríbete