¡Has copiado correctamente la URL del trabajo en el portapapeles!

Detalles del empleo 

Tipo de empleo: 

Full-Time

Ubicación:

Bengaluru, Karnataka, India

Categoría del empleo:

Field Operations

Número de empleo:

WD30230010

¡Has copiado correctamente la URL del trabajo en el portapapeles!

Descripción del empleo

Job Description

Responsibility

Expectations

Preparation of Project schedule 

Prepare project schedule with clearly defined critical path and milestone and highlight clearance required from customer

Resource and subcon deployment

Ensure competent resources are deployed at site to handle project effectively. Efficient and competent subcon with adequate manpower is deployed to meet the project timeline

Monitoring site Progress - Planned Vs Actual

Review the design and construction progress with design and project  team weekly and may be daily depending on volume and complexity of the project.  Site walk with Project engineer to monitor the site progress in line with schedule

Quality check and audits

During site walk check for quality of installation. Ensure audits done periodically and findings are addressed on immediate basis. Ensure project engineer do not repeat the findings of audit.

Coordination with cross functional team like design , SCM,L&D, Quality & finance

Coordinate with internal stake holders to ensure project deliveries are met. Highlight to next level in organization if any support required to ensure project timelines are not hampered.

Maintain Project Cash Flow – AR Collections

Timely invoicing / AR collection/ Account statement is maintained for each project.

Project completion and hand over

Pre-commissioning check to be done before T&C. Ask for any technical or resource support to ROM/AOM in advance. Start preparing O&M, As built, manual during Pre-commissioning stage only.

Trainings / Experience/Hands on experience.

With Certification on Security, FAPA & FS and BMS will be value add or should have relevant experiences in this doma

Mantente actualizado con las últimas oportunidades

Subscríbete a nuestro boletín de empleo para recibir las últimas actualizaciones sobre oportunidades profesionales, noticias de la empresa y perspectivas de la industria.

Subscríbete